Channel Studio TDL

Channel Model Presets

You can set the preset preferences for the fading profile by clicking the Channel Model Presets option.

On clicking OK in the Channel Model Presets dialog, a new fading profile configuration is created with parameters preset to the values defined in the related 3GPP test specs. You can then customize these parameters, if needed.

SCPI Command

[:SOURce]:RADio:CSTDl:FADing:CHANnel:MODel:PRESet "MIMOOrderTx:<integer>,MIMOOrderRx:<integer>,Standard:NR5G|LTE|NRNTN,ChannelModel:STATic|EPA|ETU|EVA|TDLA10|TDLA30|TDLA100|TDLB100|TDLC300|TDLD10|TDLD30|TDLC5|TDLC60,CorrelationMatrix:NONE|LOW|MEDium|MEDA|XPMED|HIGH|XPHIGH,DopplerShift:<integer>"

SCPI Example

:RADio:CSTDl:FADing:CHANnel:MODel:PRESet "MIMOOrderTx:1,MIMOOrderRx:1,Standard:NR5G,ChannelModel:STATic,CorrelationMatrix:NONE,DopplerShift:0"

Couplings

 

Preset

 

State Saved

No

Initial S/W Revision

A.19.00

Modified S/W Version

A.19.03

  • Added Medium X-pol and High X-pol for CorrelationMatrix

  • Added 16 as the supported option for MIMOOrderRx

Use Standard Doppler Shift

No SCPI, GUI only

By default, this checkbox is selected.

SCPI Command

N/A

Preset

ON

State Saved

No

Initial S/W Revision

A.19.03